5 Appendix 4: Running the TCL Script
(Ask a Question)TCL scripts are provided in the design files folder under directory HW. If required, the design flow can be reproduced from Design Implementation till generation of job file.
To run the TCL script, perform the following steps:
- Launch the Libero® SoC.
- Select
- Click Browse and
select
script.tclfrom the downloadedHWdirectory. - In order to enable FHB provide argument
FHB_ENABLEin the Arguments tab.Figure 5-1. Enabling FHB - Click Run.
After successful execution of the TCL script, Libero project is created within HW directory. For more information about TCL scripts, see mpf_an4594_df/HW/TCL_Script_readme.txt.
For more information about TCL commands, see Tcl Commands Reference Guide. For any queries encounter while running the TCL script, contact Technical Support.