2.11 Application (Core 0) Reset with Metrology (Core 1) Running Application Example
The Dual Core architecture allows some interesting functionality for an electricity meter, like the possibility to restart the Core 0 while the Core 1 continues running the metrology library, so taking measurements and generating pulses.
The Demo Meter application includes an example showing how Core 1 is able to continue
working while Core 0 is being reset. The process is divided into two steps:
- First, when the Demo Meter
Application starts, it detects the source of the reset to decide whether only
the Core 0 or the two cores must be initialized. This way it is possible to
customize the behavior depending on the reset type. For example, a watchdog
reset could re-initialize just Core 0, but a software reset could require the
initialization of the two cores.Note: Depending on the version, the Demo Meter application allows a watchdog reset to be forced using the buttons. The user presses the Scroll-down button, and then without releasing it the Scroll-up button is pressed.
- Second, the Demo Meter application code includes a dual initialization system because if the Core 1 is not reset, then some critical actions affecting Core 1 initialization must not be executed. For example, the Core 1 clock system initialization or the copy of the metrology binary from Flash to the Core 1 memory.