MCC Melody Design Patterns Introduction
Different ways to organize main.c and other application-level files.
The control flow of a microcontroller (MCU) refers to the sequence of tasks that its
Central Processing Unit (CPU) works on. The main.c and other
application level code manage the control flow in a microcontroller. This document
describes some of the most common control flow patterns and implementation
considerations for building projects using MCC Melody API.
- 100 ms Timer: Configures a timer to toggle an LED at a period of 100 ms
- UART Control Commands: Implement a basic Command Line Interface (CLI) to turn an LED ‘ON’ or ‘OFF’
- ADC Basic Printf: An ADC sample is taken every 500 ms, and the result is sent to a PC terminal
Moving beyond these simple examples to a more complex and complete embedded application, e.g., by combining a number of these building blocks, will require deliberate decisions on how the application control flow is structured. As an application grows, e.g., by adding new features, it may pass through certain complexity thresholds, at which point the most suitable control flow design pattern may change. Ideally, at this point, the application should be refactored.
- Polled control flow (blocking) - This sequential form of control flow waits for each task to be complete before moving on to the next. It is the simplest form of control flow but can be inefficient in terms of both CPU usage and power consumption. The software continuously checks (or polls) the status of a device and waits (blocks) until a specific condition is met or an operation is completed. During this waiting period, the system does not perform other tasks, dedicating its resources entirely to monitoring the device’s status.
- Interrupt/Callback-based control flow (non-blocking) - Tasks performed by the system are triggered by different events without continuous CPU involvement, i.e., this is a form of Event-Driven Programming. Interrupts are used to immediately respond to events, temporarily pausing the main program. Callbacks are specific functions invoked in response to these interrupts, providing a structured way to handle the interrupt-triggered events.
- State Machine-based control flow - Each application task has its control loop consisting of a series of states. Transitions between these states based on internal or external events provide a clear, organized structure to handle application logic predictably. It is possible to poll (block) state transitions and use interrupts/callbacks for quick events. This approach primarily focuses on the internal state and logic of the application.
- Low Power - Some of these approaches are better suited to achieving an ultra-low power embedded application. However, within each category, steps to achieve lower power are considered.
-
Polled code with callbacks: Some Melody Components generate a task routine for Polling mode. The non-blocking task routines check a relevant interrupt flag before calling a callback function. See Task Routines.
-
Polled code with interrupt/callback: For critical tasks that require immediate attention, such as if there is a hardware Fault or a real-time event that quickly must be handled while the application is polling for something else, an interrupt can be used to trigger a polling routine to make a quick response to the event.
-
Data Sheet Module Structure and Naming Conventions.
-
Modules Representation in Header Files.
-
Writing code to configure registers.
-
Application example to show alternative ways of writing code.