8 Write Sequence
In order to program the AT25010B/AT25020B/AT25040B, two separate
instructions must be executed. First, the device must be write enabled via the
Write Enable (
WREN) instruction. Then, one of the two possible write
sequences described in this section may be executed. Note: If the WP
pin is brought low or the device is not Write Enabled (
WREN), the
device will ignore the WRITE instruction and will return to the
standby state when CS is brought high. A new
CS assertion is required to re-initiate
communication.The address of the memory location(s) to be programmed must be outside the protected
address field location selected by the block write protection level. During an internal
write cycle, all commands will be ignored except the
RDSR instruction.
Refer to Table 8-1 for the address bits for AT25010B/AT25020B/AT25040B.| Address | AT25010B | AT25020B | AT25040B |
|---|---|---|---|
| AN | A6-A0 | A7-A0 | A8-A0 |
| Don’t Care Bits | A7 | None | None |