16 Building Applications Using MCC
The Microchip Code Configurator (MCC) helps to select and configure software components for the Microchip microcontrollers. The Touch project can be created using MCC. The user can add sensors and configure Touch parameters represented in graphical ways. MCC is part of Microchip's MPLAB X IDE, links for reference:
www.microchip.com/en-us/tools-resources/develop/mplab-x-ide
www.microchip.com/en-us/tools-resources/configure/mplab-code-configurator
Refer to the following link for creating touch projects using the MCC's: