3.7.1 CLC5
Configure CLC5 as shown in Figure 3-9. Select 4-input AND in the Mode field. Select the three input signals as highlighted in the red circles, the default CLCIN0, CLC3_OUT, and CLC1_OUT. The CLC logic gate 1 has output NOT as highlighted in the red circle. Make sure logic gate 2, 3, and 4 has the correct two inputs connected and also inverted. The four signals are then logically ANDed with the value inverted as output. The CLC5 logic functions as pair ANDed of the three inputs and then ORed.