18.3.2 Alternate Functions of Port C

The Port C pins with alternate functions are shown in the table below:

Table 18-6. Port C Pins Alternate Functions
Port PinAlternate Function
PC6RESET (Reset pin)

PC5ADC5 (ADC Input Channel 5)

SCL (Two-wire Serial Bus Clock Line)

PC4ADC4 (ADC Input Channel 4)

SDA (Two-wire Serial Bus Data Input/Output Line)

PC3ADC3 (ADC Input Channel 3)
PC2ADC2 (ADC Input Channel 2)
PC1ADC1 (ADC Input Channel 1)
PC0ADC0 (ADC Input Channel 0)

The alternate pin configuration is as follows:

• RESET – Port C, Bit 6

RESET, Reset pin: When the RSTDISBL Fuse is programmed, this pin functions as a normal I/O pin, and the part will have to rely on Power-on Reset and Brown-out Reset as its reset sources. When the RSTDISBL Fuse is unprogrammed, the reset circuitry is connected to the pin, and the pin can not be used as an I/O pin.

If PC6 is used as a reset pin, DDC6, PORTC6 and PINC6 will all read 0.

• SCL/ADC5 – Port C, Bit 5

SCL, Two-wire Serial Interface Clock: When the TWEN bit in TWCR is set (one) to enable the Two-wire Serial Interface, pin PC5 is disconnected from the port and becomes the Serial Clock I/O pin for the Two-wire Serial Interface. In this mode, there is a spike filter on the pin to suppress spikes shorter than 50 ns on the input signal, and the pin is driven by an open drain driver with slew-rate limitation.

PC5 can also be used as ADC input Channel 5. Note that ADC input channel 5 uses digital power.

• SDA/ADC4 – Port C, Bit 4

SDA, Two-wire Serial Interface Data: When the TWEN bit in TWCR is set (one) to enable the Two-wire Serial Interface, pin PC4 is disconnected from the port and becomes the Serial Data I/O pin for the Two-wire Serial Interface. In this mode, there is a spike filter on the pin to suppress spikes shorter than 50 ns on the input signal, and the pin is driven by an open drain driver with slew-rate limitation.

PC4 can also be used as ADC input Channel 4. Note that ADC input channel 4 uses digital power.

• ADC3 – Port C, Bit 3

PC3 can also be used as ADC input Channel 3. Note that ADC input channel 3 uses analog power.

• ADC2 – Port C, Bit 2

PC2 can also be used as ADC input Channel 2. Note that ADC input channel 2 uses analog power.

• ADC1 – Port C, Bit 1

PC1 can also be used as ADC input Channel 1. Note that ADC input channel 1 uses analog power.

• ADC0 – Port C, Bit 0

PC0 can also be used as ADC input Channel 0. Note that ADC input channel 0 uses analog power.

The tables below relate the alternate functions of Port C to the overriding signals shown in figure Figure 18-5.

Table 18-7. Overriding Signals for Alternate Functions in PC6:PC4
Signal
NamePC6/RESETPC5/SCL/ADC5PC4/SDA/ADC4
PUOERSTDISBLTWENTWEN
PUOV1PORTC5 • PUDPORTC4 • PUD
DDOERSTDISBLTWENTWEN
DDOV0SCL_OUTSDA_OUT
PVOE0TWENTWEN
PVOV000
DIEOERSTDISBL00
DIEOV000
DI–––
AIORESET INPUTADC5 INPUT / SCL INPUTADC4 INPUT / SDA INPUT
Table 18-8. Overriding Signals for Alternate Functions in PC3:PC0(1)
Signal
NamePC3/A11PC2/A10PC1/A9PC0/A8
PUOE0000
PUOV0000
DDOE0000
DDOV0000
PVOE0000
PVOV0000
DIEOE0000
DIEOV0000
DI––––
AIOADC3 INPUTADC2 INPUTADC1 INPUTADC0 INPUT
Note: 1. When enabled, the Two-wire Serial Interface enables slew-rate controls on the output pins PC4 and PC5. This is not shown in the figure. In addition, spike filters are connected between the AIO outputs shown in the port figure and the digital logic of the TWI module.