29.9.3 Data Polling EEPROM
When a new byte has been written and is being programmed into EEPROM, reading the address location being programmed will give the value 0xFF. At the time the device is ready for a new byte, the programmed value will read correctly. This is used to determine when the next byte can be written. This will not work for the value 0xFF, but the user should have the following in mind: As a chip-erased device contains 0xFF in all locations, programming of addresses that are meant to contain 0xFF, can be skipped. This does not apply if the EEPROM is Reprogrammed without chip-erasing the device. In this case, data polling cannot be used for the value 0xFF, and the user will have to wait at least tWD_EEPROM before programming the next byte. See table below for tWD_EEPROM value.
| Symbol | Minimum Wait Delay |
|---|---|
| tWD_FUSE | 4.5ms |
| tWD_FLASH | 4.5ms |
| tWD_EEPROM | 9.0ms |
| tWD_ERASE | 9.0ms |
| Instruction Format | |||||
|---|---|---|---|---|---|
| Instruction | Byte 1 | Byte 2 | Byte 3 | Byte 4 | Operation |
| Programming Enable | 1010 1100 | 0101 0011 | xxxx xxxx | xxxx
xxxx | Enable Serial Programming after RESET goes low. |
| Chip Erase | 1010 1100 | 100x xxxx | xxxx xxxx | xxxx
xxxx | Chip Erase EEPROM and Flash. |
| Read Program Memory | 0010 H000 | 0000 aaaa | bbbb bbbb | oooo oooo | Read H (high or low) data o from Program memory at word address a:b. |
| Load Program Memory Page | 0100
H000 | 0000
xxxx | xxxb
bbbb | iiii
iiii | Write H (high or low) data i to Program memory page at word address b. Data Low byte must be loaded before Data High byte is applied within the same address. |
| Write Program Memory Page | 0100 1100 | 0000 aaaa | bbbx xxxx | xxxx
xxxx | Write Program memory Page at address a:b. |
| Read EEPROM Memory | 1010 0000 | 00xx xxxa | bbbb bbbb | oooo
oooo | Read data o from EEPROM memory at address a:b. |
| Write EEPROM Memory | 1100 0000 | 00xx xxxa | bbbb bbbb | iiii
iiii | Write data i to EEPROM memory at address a:b. |
| Read Lock Bits | 0101 1000 | 0000 0000 | xxxx xxxx | xxoo
oooo | Read Lock Bits. “0” = programmed, “1” = unprogrammed. See Table Lock Bit Byte for details. |
| Write Lock Bits | 1010
1100 | 111x
xxxx | xxxx
xxxx | 11ii
iiii | Write Lock Bits. Set bits = “0” to program Lock Bits. See Table Lock Bit Byte for details. |
| Read Signature Byte | 0011 0000 | 00xx xxxx | xxxx xxbb | oooo
oooo | Read Signature Byte o at address b. |
| Write Fuse Bits | 1010 1100 | 1010 0000 | xxxx
xxxx | iiii
iiii | Set bits = “0” to program, “1” to unprogram. See Table Fuse Low Byte for details. |
| Write Fuse High Bits | 1010 1100 | 1010 1000 | xxxx
xxxx | iiii
iiii | Set bits = “0” to program, “1” to unprogram. See Table Fuse High Byte for details. |
| Read Fuse Bits | 0101 0000 | 0000 0000 | xxxx
xxxx | oooo
oooo | Read Fuse Bits. “0” = programmed, “1” = unprogrammed. See Table Fuse Low Byte for details. |
| Read Fuse High Bits | 0101 1000 | 0000 1000 | xxxx
xxxx | oooo
oooo | Read Fuse high bits. “0” = programmed, “1” = unprogrammed. See Table Fuse High Byte for details. |
| Read Calibration Byte | 0011 1000 | 00xx xxxx | 0000 00bb | oooo
oooo | Read Calibration Byte |
a = address high bits
b = address low bits
H = 0 – Low byte, 1 – High byte
o = data out
i = data in
x = don’t care