In this section, some pins of this device
are referenced by signal names describing their functionality during parallel
programming, please refer to the following figure and table Pin Name Mapping in
this section. Pins not described in the following table are referenced by pin names.
The XA1/XA0 pins determine the action
executed when the XTAL1 pin is given a positive pulse. The bit coding is shown in the
table XA1 and XA0 Coding in this section.
When pulsing WR
or OE, the command loaded determines the action executed. The
different Commands are shown in the table Command Byte Bit Coding in this
section.
Figure 29-1. Parallel Programming
Table 29-8. Pin Name Mapping
Signal
Name in Programming Mode
Pin
Name
I/O
Function
RDY/BSY
PD1
O
0:
Device is busy programming, 1: Device is ready for new command