2.3.11 Captures
The sensor data files you add to a Project are called Captures. A Capture can contain multiple time series columns corresponding to different devices, sensors, channels or axes, as long as all of the columns in the capture describe the same period of time.
Examples:
# to list all capture files
client.list_captures()
my_capture = client.project.captures.get_capture_by_filename("Capture Name")
my_capture = client.project.captures.get_capture_by_uuid(uuid)
- class mplabml.datamanager.captures. Captures(connection, project)
Base class for a collection of Captures
- build_capture_list()
Populates the function_list property from the server
- create_capture(filename, filepath, asynchronous=True, capture_info=None)
Creates a capture object from the given filename and filepath
- Parameters
filename (str) – Desired name of the file on the server
filepath (str) – Local path to the file to be uploaded
asynchronous (bool) – Whether to process asynchronously
- Returns
capture object
- Raises
CaptureExistsError , if the Capture already exists on the server –
- get_capture_by_filename(filename)
Gets a capture object from the server using its filename property
- Parameters
filename (str) – the capture’s name
- Returns
Capture object or None if it does not exist
- get_capture_by_uuid(uuid)
Gets a capture object from the server using its filename property
- Parameters
filename (str) – The capture’s name
- Returns
Capture object or None if it does not exist
- get_captures()
Gets all captures from the server
- Returns
List of captures for the project
- get_captures_by_metadata(key, value)
Gets captures by existing metadata key-values
- Parameters
key (str) – The name of the metadata item
value (str , int , or float) – The value to search for
- Returns
List of captures that have the desired metadata key-value pair
- get_label_names()
Gets all the label names within a project
- Returns
list of label names
- get_label_names_and_values()
Gets all the label names and possible values for a project
- Returns
List(dict) containing metadata names and values
- get_metadata_names()
Gets all the metadata names within a project
- Returns
list of metadata names
- get_metadata_names_and_values()
Gets all the metadata names and possible values for a project
- Returns
List(dict) containing metadata names and values
- get_statistics()
Gets all capture statistics for the project
- Returns
DataFrame of capture statistics
- class mplabml.datamanager.capture. Capture(connection, project, filename='', path='', uuid='', capture_configuration_uuid=None, capture_info=None, created_at=None, **kwargs)
Base class for a Capture
- await_ready(sleep=3, retries=0)
Blocks until Capture (Capture) is ready or failed
- Parameters
sleep (int) – Number of seconds to sleep between polling
retries (int) – Number of times to retry before unblocking and returning False. Use 0 for infinite.
- Returns
None or raises CaptureUploadFailureError if upload failed
- property capture_info
Info about capture
- delete()
Calls the REST API to delete the capture from the server
- classmethod initialize_from_dict(capture_dict)
Reads a dictionary or properties and populates a single capture
- Parameters
capture_dict (dict) – Contains the capture’s ‘name’ property
- Returns
capture object
- insert(asynchronous=False)
Calls the REST API to insert a new Capture
- property path
The local or server path to the Capture file data
- property ready
Returns if Capture (Capture) is ready or not
- Returns
True if task is ready or False if task is pending. Raises Exception if task failed.
- Return type
Boolean
- refresh()
Calls the REST API and self populates properties from the server
- update()
Calls the REST API to update the capture
- property uuid
Auto-generated unique identifier for the Capture object