6.2.6.3.4 DMA Interrupt Generation
The DMA Controller operation sets the following interrupt flags in the layer Interrupt Status registers:
- END—indicates that the current frame DMA transfer is completed.
- ERROR—indicates that a bus transfer error has been detected.
- OVF—indicates that a DMA transfer is still pending at the end of frame.