7.2 Page Write
A page write operation for the AT24C01C and AT24C02C allows up to eight bytes to be written in the same write cycle, provided all bytes are in the same row of the memory array (where address bits A6/A7 to A3 are the same). Partial page writes of less than eight bytes are also allowed.
A page write operation for the AT24C04C and AT24C08C allows up to 16 bytes to be written in the same write cycle, provided all bytes are in the same row of the memory array (where address bits A8/A9 to A4 are the same). Partial page writes of less than 16 bytes are also allowed.
A page write is initiated the same way as a byte write, but the bus host does not send a Stop condition after the first data word is clocked in. Instead, after the EEPROM acknowledges receipt of the first data word, the bus host can transmit up to seven (AT24C01C/AT24C02C) or fifteen (AT24C04C/AT24C08C) additional data words. The EEPROM will respond with an ACK after each data word is received. Once all data to be written have been sent to the device, the bus host must issue a Stop condition (see Figure 7-2) at which time the internally self-timed write cycle will begin.
The lower three (AT24C01C/AT24C02C) or four (AT24C04C/AT24C08C) bits of the word address are internally incremented following the receipt of each data word. The higher order address bits are not incremented and retain the memory page row location. Page write operations are limited to writing bytes within a single physical page, regardless of the number of bytes actually being written. When the incremented word address reaches the page boundary, the address counter will roll over to the beginning of the same page. Nevertheless, creating a rollover event should be avoided as previously loaded data in the page could become unintentionally altered.
- For the AT24C01C, AT24C02C and AT24C04C, the @ indicates the A1 hardware client address bit. For the AT24C08C, the @ indicates the A9 word address bit.
- For the AT24C01C and AT24C02C, the $ indicates the A0 hardware client address bit. For the AT24C04C and AT24C08C, the $ indicates the A8 word address bit.
- For the AT24C01C, the % indicates a “don’t care” bit. For the AT24C02C, AT24C04C and AT24C08C, the % indicates the A7 word address bit.