1.5.4.5 AL_Tasks Function
C
void AL_Tasks (
SYS_MODULE_OBJ object
);
Summary
Routine that maintains the state machine in the AL module.
Description
Routine that performs the tasks necessary to maintain the state machine in the Meters And More AL module.
Parameters
| Param | Description |
|---|---|
| object | Handle to the module instance, as returned from AL_Initialize Function |
Returns
None.
Example
SYS_MODULE_OBJ sysObjMetersandmore;
AL_INIT alInitData = {
.taskRateMs = 5U,
.isMaster = false
};
sysObjMetersandmore = AL_Initialize(0, (SYS_MODULE_INIT *)&dllInitData);
AL_Tasks(sysObjMetersandmore);
Remarks
It is called from System Initialize module. User Application does not need to call this function.