1.5.4.20 AL_EventIndicationCallbackRegister Function
C
AL_RESULT AL_EventIndicationCallbackRegister (
AL_EVENT_IND_CALLBACK callback
);
Summary
Allows a client to set a Meters And More AL Event.indication event handling function for the module to call back when AL generates a new event.
Description
This function allows a client to register a Meters And More AL Event.indication event handling function for the module to call back when a Meters And More AL event occurs.
Parameters
| Param | Description |
|---|---|
| callback | Pointer to the callback function. See AL_EVENT_IND_CALLBACK Typedef. |
Returns
Result of Callback setting.
Example
void APP_Event_Ind_callback(AL_EVENT_IND_CALLBACK *indParams)
{
if (indParams->eventId == AL_EVENT_ID_MAC_ACA){
/* Process Event */
}
}
AL_EventIndicationCallbackRegister(APP_Event_Ind_callback);
Remarks
Callback can be set to a NULL pointer to stop receiving notifications.
This Callback is only generated in Master node. There is no need to set a handling function on Slave nodes.