1.5.4.12 AL_DATA_CONFIRM_CALLBACK Typedef

C

typedef void ( *AL_DATA_CONFIRM_CALLBACK )( AL_DATA_CONFIRM_PARAMS *cfmParams );

Summary

Pointer to a Meters And More AL module Data Confirm Function Pointer.

Description

This data type defines the required function signature for the Meters And More AL module Data Confirm callback function. A client must register a pointer using the callback register function whose function signature (parameter and return value types) match the types specified by this function pointer in order to receive related event callbacks from the module.

Parameters

ParamDescription
cfmParamsPointer to the object containing data related to the result of last transmission. See AL_DATA_CONFIRM_PARAMS Struct.

Returns

None.

Example

    void APP_MyDataCfmEventHandler( AL_DATA_CONFIRM_PARAMS *cfmParams )
    {
        switch(cfmParams->txStatus)
        {
            case AL_TX_STATUS_SUCCESS:
                /* Successful transmission */
                break;
            default:
                /* Transmission failed */
                break;
        }
    }

Remarks

None.