1.2.4.5 DLL_Tasks Function
C
void DLL_Tasks (
SYS_MODULE_OBJ object
);
Summary
Routine that maintains the state machine in the DLL module.
Description
Routine that performs the tasks necessary to maintain the state machine in the Meters And More DLL module.
Parameters
| Param | Description |
|---|---|
| object | Handle to the module instance, as returned from DLL_Initialize Function |
Returns
None.
Example
SYS_MODULE_OBJ sysObjMetersandmore;
DLL_INIT dllInitData = {
.taskRateMs = 1U,
.isMaster = false
};
sysObjMetersandmore = DLL_Initialize(0, (SYS_MODULE_INIT *)&dllInitData);
DLL_Tasks(sysObjMetersandmore);
Remarks
It is called from System Initialize module. User Application does not need to call this function.