5.3 Component Selection
Knowing the poles, zeros and the appropriate amplification factor, the rest of the components in the compensation network can be calculated.
The gain is set by the ratio between Rcomp and RFBT. As RFBT and AVM are set previously, Rcomp can be calculated as the product of these:
Setting the first zero of the amplifier is done using Ccomp and Rcomp, while the other is set by CFF and RFBT. These will fall on the output filter poles, resulting in the following capacitor values:
The first pole of the amplifier is set by the combination of CHF and Rcomp, and the second is set using RFF and CFF. Setting the pole resulting from CHF and Rcomp equal to half the switching frequency, fSW, and the pole resulting from CFF and RFF equal to the zero generated by the output capacitor and its series resistance gives the following equations for CHF and RFF: