SRV_PCOUP_Get_Config Function
C
SRV_PLC_PCOUP_DATA * SRV_PCOUP_Get_Config(SRV_PLC_PCOUP_BRANCH branch);
Summary
Get the PLC PHY Coupling parameters for the specified transmission branch.
Description
This function allows to get the PLC PHY Coupling parameters for the specified transmission branch. These parameters can be sent to the PLC device through PLC Driver PIB interface (DRV_PLC_PHY_PIBSet or DRV_G3_MACRT_PIBSet).
Precondition
None.
Parameters
| Param | Description |
|---|---|
| branch | Transmission branch (SRV_PLC_PCOUP_BRANCH Enum) for which the parameters are requested |
Returns
Pointer to SRV_PLC_PCOUP_DATA Struct, containing the PLC PHY Coupling parameters
if branch parameter is valid
NULL
if branch parameter is not valid
Example
SRV_PLC_PCOUP_DATA *pCoupValues; pCoupValues = SRV_PCOUP_Get_Config(SRV_PLC_PCOUP_MAIN_BRANCH);
Remarks
This function is only generated by MCC if the PLC Driver uses G3-PLC PHY.
If SRV_PCOUP_Set_Config function is used to set the PLC PHY Coupling parameters, this function is not needed.