SRV_PCOUP_Get_Phy_Band Function
C
uint8_t SRV_PCOUP_Get_Phy_Band(SRV_PLC_PCOUP_BRANCH branch);Summary
Get the G3-PLC PHY band associated to the specified transmission branch.
Description
This function allows to get the G3-PLC PHY band associated to the specified transmission branch.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| branch | Transmission branch (SRV_PLC_PCOUP_BRANCH Enum) for which the PHY band is requested |
Returns
G3-PLC PHY band associated to the specified transmission branch (see drv_plc_phy_comm.h or drv_g3_macrt_comm.h):
0: G3_CEN_A
1: G3_CEN_B
2: G3_FCC
3: G3_ARIB
0xFF: G3_INVALID (if transmission branch is not valid)
Example
uint8_t phyBand;
phyBand = SRV_PCOUP_Get_Phy_Band(SRV_PLC_PCOUP_MAIN_BRANCH);
if (phyBand == G3_CEN_A)
{
// G3 CEN-A band
}Remarks
This function is only generated by MCC if the PLC Driver uses G3-PLC PHY.