SRV_PCOUP_Set_Config Function
C
bool SRV_PCOUP_Set_Config(DRV_HANDLE handle, SRV_PLC_PCOUP_BRANCH branch);Summary
Set the PLC PHY Coupling parameters for the specified transmission branch.
Description
This function allows to set the PLC PHY Coupling parameters for the specified transmission branch, using the PLC Driver PIB interface (DRV_PLC_PHY_PIBSet or DRV_G3_MACRT_PIBSet).
Precondition
The PLC driver's open routine (DRV_PLC_PHY_Open or DRV_G3_MACRT_Open) must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid instance handle, returned from the PLC driver's open routine |
| branch | Transmission branch (SRV_PLC_PCOUP_BRANCH Enum) for which the parameters will be set |
Returns
true
Successful configuration
false
if branch parameter is not valid
if there is an error when using the PLC Driver PIB interface
Example
// 'handle', returned from DRV_PLC_PHY_Open or DRV_G3_MACRT_Open bool result; result = SRV_PCOUP_Set_Config(handle, SRV_PLC_PCOUP_MAIN_BRANCH);
Remarks
This function is only generated by MCC if the PLC Driver uses G3-PLC PHY.