1.2.8.2 Using The Library
The RF PHY Serial library is an add-on that can be used along with the RF215 Driver. The RF215 driver is the one in charge of RF communications, while the Serial library is used to serialize the PHY API, this is, to decode/encode the packets containing the RF frames, their related parameters and the PIB objects, after receiving/sending them them from/to a serial interface.
Following example illustrate how to use the Serial library (which in turn uses the USI service to send/receive the packets to/from an external tool), to serialize the RF PHY API.
Example implementation of a RF PHY API Serialization
APP_RF_DATA app_rfData; static uint8_t rfDataPIBBuffer[APP_RF_PIB_BUFFER_SIZE]; static void _APP_RF_RxIndCb(DRV_RF215_RX_INDICATION_OBJ* indObj, uintptr_t ctxt) { uint8_t* pSerialData; size_t length; DRV_RF215_TRX_ID trxId = (DRV_RF215_TRX_ID) ctxt; /* Serialize received message and send through USI */ pSerialData = SRV_RSERIAL_SerialRxMessage(indObj, trxId, &length); SRV_USI_Send_Message(app_rfData.srvUSIHandle, SRV_USI_PROT_ID_PHY_RF215, pSerialData, length); } static void _APP_RF_TxCfmCb ( DRV_RF215_TX_HANDLE txHandle, DRV_RF215_TX_CONFIRM_OBJ *cfmObj, uintptr_t ctxt ) { uint8_t* pSerialData; size_t length; DRV_RF215_TRX_ID trxId = (DRV_RF215_TRX_ID) ctxt; /* Serialize confirm and send through USI */ pSerialData = SRV_RSERIAL_SerialCfmMessage(cfmObj, trxId, txHandle, &length); SRV_USI_Send_Message(app_rfData.srvUSIHandle, SRV_USI_PROT_ID_PHY_RF215, pSerialData, length); } void _APP_RF_UsiPhyProtocolEventCb(uint8_t *pData, size_t usiLength) { uint8_t* pSerialData; size_t length; SRV_RSERIAL_COMMAND command; DRV_HANDLE rf215Handle; DRV_RF215_TRX_ID trxId; DRV_RF215_PIB_ATTRIBUTE pibAttr; DRV_RF215_PIB_RESULT pibResult; uint8_t pibSize, pibSizePhy; /* Protection for invalid length */ if (usiLength == 0) { return; } /* Process received message from PLC Tool */ command = SRV_RSERIAL_GetCommand(pData); switch (command) { case SRV_RSERIAL_CMD_PHY_GET_CFG: { /* Extract PIB information */ SRV_RSERIAL_ParsePIB(pData, &trxId, &pibAttr, &pibSize); pibSizePhy = DRV_RF215_GetPibSize(pibAttr); if (pibSize >= pibSizePhy) { if (trxId == RF215_TRX_ID_RF09) { rf215Handle = app_rfData.rf215HandleRF09; } else { rf215Handle = app_rfData.rf215HandleRF24; } /* Get PIB from RF215 driver */ pibResult = DRV_RF215_GetPib(rf215Handle, pibAttr, rfDataPIBBuffer); } else { /* Invalid length */ pibResult = RF215_PIB_RESULT_INVALID_PARAM; } /* Serialize PIB get response and send through USI */ pSerialData = SRV_RSERIAL_SerialGetPIB(trxId, pibAttr, pibSize, pibResult, rfDataPIBBuffer, &length); SRV_USI_Send_Message(app_rfData.srvUSIHandle, SRV_USI_PROT_ID_PHY_RF215, pSerialData, length); } break; case SRV_RSERIAL_CMD_PHY_SET_CFG: { uint8_t *pPibValue; /* Extract PIB information */ pPibValue = SRV_RSERIAL_ParsePIB(pData, &trxId, &pibAttr, &pibSize); pibSizePhy = DRV_RF215_GetPibSize(pibAttr); if (pibSize >= pibSizePhy) { if (trxId == RF215_TRX_ID_RF09) { rf215Handle = app_rfData.rf215HandleRF09; } else { rf215Handle = app_rfData.rf215HandleRF24; } /* Get PIB from RF215 driver */ pibResult = DRV_RF215_SetPib(rf215Handle, pibAttr, pPibValue); } else { /* Invalid length */ pibResult = RF215_PIB_RESULT_INVALID_PARAM; } /* Serialize PIB set response and send through USI */ pSerialData = SRV_RSERIAL_SerialSetPIB(trxId, pibAttr, pibSize, pibResult, &length); SRV_USI_Send_Message(app_rfData.srvUSIHandle, SRV_USI_PROT_ID_PHY_RF215, pSerialData, length); } break; case SRV_RSERIAL_CMD_PHY_SEND_MSG: { bool txCancel; DRV_RF215_TX_REQUEST_OBJ txReq; DRV_RF215_TX_HANDLE txHandle; /* Parse TRX identifier from USI */ trxId = SRV_RSERIAL_ParseTxMessageTrxId(pData); if (trxId == RF215_TRX_ID_RF09) { rf215Handle = app_rfData.rf215HandleRF09; } else { rf215Handle = app_rfData.rf215HandleRF24; } /* Parse TX request data from USI */ txCancel = SRV_RSERIAL_ParseTxMessage(pData, &txReq, &txHandle); if (txCancel == false) { DRV_RF215_TX_RESULT txResult; /* Send Message through RF */ txHandle = DRV_RF215_TxRequest(rf215Handle, &txReq, &txResult); SRV_RSERIAL_SetTxHandle(txHandle); if (txResult != RF215_TX_SUCCESS) { DRV_RF215_TX_CONFIRM_OBJ txCfm; txCfm.txResult = txResult; txCfm.ppduDurationUS = 0; txCfm.timeIni = SYS_TIME_Counter64Get(); /* TX request error */ _APP_RF_TxCfmCb(DRV_RF215_TX_HANDLE_INVALID, &txCfm, (uintptr_t) trxId); } } else { /* Cancel TX request */ DRV_RF215_TxCancel(rf215Handle, txHandle); } } break; default: break; } } void APP_Initialize(void) { /* Place the App state machine in its initial state. */ app_rfData.state = APP_RF_STATE_INIT; /* Initialize handles */ app_rfData.rf215HandleRF09 = DRV_HANDLE_INVALID; app_rfData.rf215HandleRF24 = DRV_HANDLE_INVALID; app_rfData.srvUSIHandle = DRV_HANDLE_INVALID; app_rfData.tmr1Handle = SYS_TIME_HANDLE_INVALID; } void APP_Tasks(void) { /* Check the application's current state. */ switch ( app_rfData.state ) { /* Application's initial state. */ case APP_RF_STATE_INIT: { /* Check status of RF215 driver */ SYS_STATUS rf215Status = DRV_RF215_Status(sysObj.drvRf215); if (rf215Status == SYS_STATUS_READY) { /* RF215 driver is ready to be opened */ app_rfData.rf215HandleRF09 = DRV_RF215_Open(DRV_RF215_INDEX_0, RF215_TRX_ID_RF09); app_rfData.rf215HandleRF24 = DRV_RF215_Open(DRV_RF215_INDEX_0, RF215_TRX_ID_RF24); if (app_rfData.rf215HandleRF09 != DRV_HANDLE_INVALID) { /* Register RF215 driver callbacks */ DRV_RF215_RxIndCallbackRegister(app_rfData.rf215HandleRF09, _APP_RF_RxIndCb, (uintptr_t) RF215_TRX_ID_RF09); DRV_RF215_TxCfmCallbackRegister(app_rfData.rf215HandleRF09, _APP_RF_TxCfmCb, (uintptr_t) RF215_TRX_ID_RF09); } if (app_rfData.rf215HandleRF24 != DRV_HANDLE_INVALID) { /* Register RF215 driver callbacks */ DRV_RF215_RxIndCallbackRegister(app_rfData.rf215HandleRF24, _APP_RF_RxIndCb, (uintptr_t) RF215_TRX_ID_RF24); DRV_RF215_TxCfmCallbackRegister(app_rfData.rf215HandleRF24, _APP_RF_TxCfmCb, (uintptr_t) RF215_TRX_ID_RF24); } if ((app_rfData.rf215HandleRF09 != DRV_HANDLE_INVALID) || (app_rfData.rf215HandleRF24 != DRV_HANDLE_INVALID)) { /* Open USI Service */ app_rfData.srvUSIHandle = SRV_USI_Open(SRV_USI_INDEX_1); if (app_rfData.srvUSIHandle != DRV_HANDLE_INVALID) { /* Set Application to next state */ app_rfData.state = APP_RF_STATE_CONFIG_USI; } else { /* Set Application to ERROR state */ app_rfData.state = APP_RF_STATE_ERROR; } } else { /* Set Application to ERROR state */ app_rfData.state = APP_RF_STATE_ERROR; } } else if (rf215Status == SYS_STATUS_ERROR) { /* Set Application to ERROR state */ app_rfData.state = APP_RF_STATE_ERROR; } break; } case APP_RF_STATE_CONFIG_USI: { SRV_USI_STATUS usiStatus = SRV_USI_Status(app_rfData.srvUSIHandle); if (usiStatus == SRV_USI_STATUS_CONFIGURED) { /* Register USI callback */ SRV_USI_CallbackRegister(app_rfData.srvUSIHandle, SRV_USI_PROT_ID_PHY_RF215, _APP_RF_UsiPhyProtocolEventCb); /* Set Application to next state */ app_rfData.state = APP_RF_STATE_READY; } else if (usiStatus == SRV_USI_STATUS_ERROR) { /* Set Application to ERROR state */ app_rfData.state = APP_RF_STATE_ERROR; } break; } case APP_RF_STATE_READY: { /* Check USI status in case of USI device has been reset */ if (SRV_USI_Status(app_rfData.srvUSIHandle) == SRV_USI_STATUS_NOT_CONFIGURED) { /* Set Application to next state */ app_rfData.state = APP_RF_STATE_CONFIG_USI; } break; } case APP_RF_STATE_ERROR: { /* Handle error in application's state machine */ break; } /* The default state should never be executed. */ default: { break; } } }