2.7.3.1 AbortCodeGet()

static ftp_abort_code_t AbortCodeGet (bl_result_t targetStatus)[static]

Converts the given result codes into MDFU protocol defined data values.

This function converts the bootloader core result codes into codes that are defined by the MDFU protocol.

Parameters:
in targetStatus

- Bootloader result code that needs to be mapped to one of the defined protocol codes

Returns:

FTP_INVALID_FILE_ERROR - The bootloader failed during file verification, either during the metadata block validation or a failed image verification

FTP_ADDRESS_ERROR - The bootloader processed a block with an invalid address

FTP_WRITE_ERROR - The bootloader encountered an error while trying to process the data. Likely be due to NVM errors

FTP_GENERIC_ERROR - The bootloader code received has not been mapped to a specific FTP abort code