3.2.1 Connecting the Flexible Flat Cable (FFC)
To connect the LCD module to the host board using the flexible flat cable (FFC), follow the
sequence below:
- First :
- Connect the FFC to the LCD module as illustrated in Figure 3-2.
- Ensure that the metallic fingers of the FFC are facing towards the interior of the board when the FFC is inserted in the header J1, as shown in Figure 3-2.
- Verify that Pin 1 of the FFC is aligned with Pin 1 of the J1 connector of the AC69T88A board.
- Second:
- Connect the FFC to the host board as illustrated in Figure 3-3.
- Ensure that the FFC metallic fingers are facing towards the outside of the board when it is inserted in the connector, as shown in Figure 3-3.
- Verify that Pin 1 of the FFC is aligned with Pin 1 of the connector.