1.1.30.3 WDRV_WINC_BSSConnect
C
WDRV_WINC_STATUS WDRV_WINC_BSSConnect
(
DRV_HANDLE handle,
const WDRV_WINC_BSS_CONTEXT *const pBSSCtx,
const WDRV_WINC_AUTH_CONTEXT *const pAuthCtx,
const WDRV_WINC_CONN_CFG *pWiFiCfg,
const WDRV_WINC_BSSCON_NOTIFY_CALLBACK pfNotifyCallback
)Description
Using the defined BSS and authentication contexts this function requests the WINC connect to the BSS as an infrastructure station.
Precondition
WDRV_WINC_Initialize must have been called.
WDRV_WINC_Open must have been called to obtain a valid handle.
A BSS context must have been created and initialized.
An authentication context must have been created and initialized.
Parameters
| Parameters | Description |
|---|---|
| handle | Client handle obtained by a call to WDRV_WINC_Open. |
| pBSSCtx | Pointer to BSS context. |
| pAuthCtx | Pointer to authentication context. |
| pWiFiCfg | Optional WiFi configuration. |
| pfNotifyCallback | Pointer to notification callback function. |
Returns
- WDRV_WINC_STATUS_OK - The request has been accepted.
- WDRV_WINC_STATUS_NOT_OPEN - The driver instance is not open.
- WDRV_WINC_STATUS_INVALID_ARG - The parameters were incorrect.
- WDRV_WINC_STATUS_REQUEST_ERROR - The request to the WINC was rejected.
- WDRV_WINC_STATUS_INVALID_CONTEXT - The BSS context is not valid.
- *WDRV_WINC_STATUS_CONNECT_FAIL - The connection has failed.
Remarks
None.