1.1.7.8 WDRV_WINC_AssocDisconnect
C
WDRV_WINC_STATUS WDRV_WINC_AssocDisconnect
(
WDRV_WINC_ASSOC_HANDLE assocHandle
)Description
This API disconnects the STA associated with softAP based on the input association handle. Association handle is updated to the application whenever a new STA is connected to the softAP.
This API can also be used in STA mode to disconnect the STA from an AP.
Precondition
WDRV_WINC_Initialize must have been called.
WDRV_WINC_Open must have been called to obtain a valid handle.
WDRV_WINC_APStart must have been called to start softAP in softAP mode.
WDRV_WINC_BSSConnect must have been called to connect to an AP in STA mode.
Parameters
| Parameters | Description |
|---|---|
| assocHandle | WDRV_WINC_ASSOC_HANDLE obtained when STA joins an AP or an association is done. |
Returns
- WDRV_WINC_STATUS_OK - The request has been accepted.
- WDRV_WINC_STATUS_NOT_OPEN - The driver instance is not open.
- WDRV_WINC_STATUS_INVALID_ARG - The parameters were incorrect.
- WDRV_WINC_STATUS_REQUEST_ERROR - The request to the WINC was rejected.
- WDRV_WINC_STATUS_NOT_CONNECTED - The association is not valid.
Remarks
This function is currently not implemented and should not be used.