5.2.2 Stop Condition
A Stop condition occurs when there is a low-to-high transition on
the SDA pin while the SCL pin is stable in the logic ‘1
’ state.
The master can use the Stop condition to end a data transfer sequence with the AT24CSW04X/AT24CSW08X, which will subsequently return to Standby mode. The master can also utilize a repeated Start condition instead of a Stop condition to end the current data transfer if the master will perform another operation. Refer to Figure 5-1 for more details.