3.1.2 Join Procedure
This section captures the power profile during the joining process with the network server, and also highlights the profile on the following modes:
- Join request sent to network server
- Join accept received in RX1 receive window
- Join accept received in RX2 receive window
The following table provides the settings for profiling the join procedure.
|
Attribute |
Value |
|---|---|
|
TX data rate |
DR0 and DR5 |
|
RX1 data rate |
Same as TX data rate |
|
RX2 data rate |
DR0 |
|
Join accept delay 1 |
5s |
|
Join accept delay 2 |
6s |
|
TX power(1) |
1 (default) |
|
Note:
| |
The following plots illustrate the transmission of the join request, reception of the join accept in the RX1 window and reception of the join accept in the RX2 at transmission data rates DR0 and DR5 followed by their respective zoomed-in plots with consumption values in each state.
From the preceding plots, the total time taken to complete the transaction at different data rate scenarios is given in the following table.
|
Data Rate |
Total Time Taken to Complete the Transaction | Units | |
|---|---|---|---|
|
Join Request Transmission and Join Accept in RX1 (Transaction Event 1) |
Join Request Transmission and Join Accept in RX2 (Transaction Event 2) | ||
|
DR0 |
8.33 |
9.35 | seconds |
|
DR5 |
5.15 |
7.90 | seconds |
- Transaction event 1 – TX_OCCURING + BEFORE_RX1 + RX1_OPEN
- Transaction event 2 – TX_OCCURING + BEFORE_RX1 + RX1_OPEN + BETWEEN_RX1_RX2 + RX2_OPEN
| Attribute | Measured Value | Units | |
|---|---|---|---|
| DR0 | DR5 | ||
|
Total duration |
1484 |
68.70 | ms |
|
Average current |
34.81 |
32.02 | mA |
|
Peak current |
37.80 |
38.02 | mA |
|
Total charge |
51658.04 |
2199.78 | mA×ms |
|
Attribute |
Measured Value | Units | |
|---|---|---|---|
|
DR0 |
DR5 | ||
|
Total duration |
4973 |
4937 | ms |
|
Average current |
1.487 |
1.548 | mA |
|
Peak current |
1.638 |
1.621 | mA |
|
Total charge |
7394.86 |
7642.48 | mA×ms |
|
Attribute |
Measured Value | Units | |
|---|---|---|---|
|
DR0 |
DR5 | ||
|
Total duration (ms) |
1878 |
134.2 | ms |
|
Average current (mA) |
13.84 |
13.41 | mA |
|
Peak current (mA) |
14.82 |
15.25 | mA |
|
Total charge (mA×ms) |
25991.52 |
1799.63 | mA×ms |
|
Attribute |
Measured Value | Units | |
|---|---|---|---|
|
DR0 |
DR5 | ||
|
Total duration |
717.9 |
949 | ms |
|
Average current |
1.440 |
1.490 | mA |
|
Peak current |
1.564 |
1.641 | mA |
|
Total charge |
1033.78 |
1414.01 | mA×ms |
|
Attribute |
Measured Value | Units | |
|---|---|---|---|
|
DR0 |
DR5 | ||
|
Total duration |
1862 |
1862 | ms |
|
Average current |
13.98 |
13.3 | mA |
|
Peak current |
16.21 |
17.05 | mA |
|
Total charge |
26030.8 |
24764.6 | mA×ms |
|
Attribute |
Measured Value | Units | |
|---|---|---|---|
|
DR0 |
DR5 | ||
|
Total duration |
265.5 |
87.61 | ms |
|
Average current |
13.87 |
13.55 | mA |
|
Peak current |
15.21 |
17.40 | mA |
|
Total charge |
3682.5 |
1187.12 | mA×ms |
The following table provides the time stamp reference for each join request sent and join accept received in RX1 and RX2 reception windows.
|
Packet N |
Packet Type |
Time Stamp |
Source |
Destination | |
|---|---|---|---|---|---|
|
DR0 |
DR5 | ||||
|
Packet 1 |
Join request 1 |
12:56:23.457 |
12:34:43.860 |
End device (WLR089) |
Network server |
|
Packet 2 |
Join accept in RX1 |
12:56:32.788 |
12:34:49.005 |
Network server |
End device (WLR089) – RX1 |
|
Packet N |
Packet Type |
Time Stamp |
Source |
Destination | |
|---|---|---|---|---|---|
|
DR0 |
DR5 | ||||
|
Packet 1 |
Join request 2 |
12:57:53.677 |
12:37:04.189 |
End device (WLR089) |
Network server |
|
Packet 2 |
Join accept in RX2 |
12:57:03.002 |
12:37:12.095 |
Network server |
End device (WLR089) – RX2 |