4.2 Operational Overview
Note: Ensure you read Power Connections, PC and Smartphone Connections and Target Connections before completing
Step 5.
To debug and program code using the MPLAB PICkit 5 In-Circuit Debugger:
- Download and install the latest MPLAB X IDE from the MPLAB X IDE webpage. MPLAB IPE is included in the MPLAB X IDE installer. See MPLAB X IDE documentation for how to create a project for developing application code and how to debug code.
- Find examples of code in MPLAB Discover or search for Microchip content on GitHub, such as Microchip PIC & AVR Examples.
- Find a compiler for on your application device on the MPLAB XC Compilers webpage.
- Purchase MPLAB PICkit 5 and optionally the Debugger Adapter Board.
- Launch MPLAB X IDE. Plug in MPLAB PICkit 5 to the computer using the USB cable. Ensure you target is correctly connected.
- Open your project or an example
project in MPLAB X IDE. Right click on the project name in
the Projects tab and select Properties. In the Project Properties dialog, ensure
that PICkit 5 is selected under
“Connected Hardware Tool”. Then select the PICkit 5 Category under a Conf(iguration) and setup options
from the “Option Categories” list. Note: This is where you select power to target if desired.
- Read the following sections for details on operation for your application device.
- For a complete list of debugger limitations for your device, see the online Help file in MPLAB X IDE (Help > Help Contents > Hardware Tool Reference Help > Limitations - Emulators and Debuggers).