6.6 Observe the Output

To observe the output on the board and in the serial terminal, follow these steps:
  1. To launch MPLAB® Data Visualizer, click the icon shown in the below image.

    Figure 6-18. Launch MPLAB Data Visualizer
  2. Select the COM port corresponding to the Curiosity Nano from the Source drop-down menu in the terminal window.

    Figure 6-19. Serial Communication Port Selection
  3. Set the baud rate to 115200 by clicking the settings icon next to the COM port.

  4. Click the play icon to view the UART Communication in the terminal window.

    Figure 6-20. Setting the Baud Rate
  5. The on-board LED of the AVR32LA32 Curiosity Nano evaluation kit toggles at a default interval of two seconds. The LED blink interval is displayed in the serial terminal.

    • Press the SW switch on the AVR32LA32 Curiosity Nano evaluation kit to change the blink interval to 400 ms
    • Each press of the on-board switch (SW0) of the Curiosity Nano evaluation kit alternates the blink interval between 400 ms and two seconds
    Figure 6-21. Output Observed on Terminal
Note: The application discussed above is implemented and available on MPLAB® Discover.