6.1 Create the First Application on the AVR® LA MCU
To create an MCC Melody-based project, follow these steps:
- Launch MPLAB® X IDE.
-
From the File menu, click New Project, or click the “New Project” icon. The New Project window will open.
Figure 6-1. Create a New Project in MPLAB®X IDE -
In the Choose Project step, select the following:
- Categories: Microchip Embedded
- Projects: Application Project(s)
Click Next
Figure 6-2. New Project Window, Project Selection -
In the Select Device step, select the following:
- Device: AVR32LA32
- Tool: AVR32LA32 Curiosity Nano
Click Next
Figure 6-3. Device and Tool Selection -
In the Select Compiler step, expand the XC8 list of options, then select the compiler (for example, XC8 v3.10). Click Next.
Figure 6-4. Compiler Selection -
In the Select Project Name and Folder step, enter the following:
- Project Name:
avr32la32 _cnano_ getting_started - Project Location:
C:\GettingStarted_With_AVRLA - The project location can be specified either by entering the path in the field or by clicking the Browse button next to the field
Click Finish
Figure 6-5. Project Name and Project Location - Project Name:
-
The project is created, and the MCC plug-in launches in a new window.
Figure 6-6. MPLAB® Code Configurator Window