35.12.1 Principle of Operation

Important: When AVDD < 2.5v, for proper operation of the analog functions on the I/O port pins it is critical that the internal charge pumps be enabled as necessary, as defined in SUPC.VREGCTRL.CPEN.

Each PORT group of up to 32 pins is controlled by the registers in PORT, as described in the figure. These registers in PORT are duplicated for each PORT group, with increasing base addresses. The number of PORT groups may depend on the package or number of pins.

Figure 35-3. Overview of the Peripheral Functions Multiplexing

The I/O pins of the device are controlled by the PORT peripheral registers. Each port pin has a corresponding bit in the Data Direction (DIR) and Data Output Value (OUT) registers to enable that pin as an output and to define the output state.

The direction of each pin in a PORT group is configured by the DIR register. If a bit in DIR is set to '1', the corresponding pin is configured as an output pin. If a bit in DIR is set to '0', the corresponding pin is configured as an input pin.

When the direction is set as output, the corresponding bit in the OUT register will set the level of the pin. If bit ‘n’ in OUT is written to '1', pin ‘n’ is driven HIGH. If bit ‘n’ in OUTx is written to '0', pin ‘n’ is driven LOW. Pin configuration can be set by the Pin Configuration (PINCFGn) registers, with n = 00, 01, ..31 representing the bit position.

The Data Input Value (IN) is set as the input value of a port pin with resynchronization to the PORT clock. To reduce power consumption, these input synchronizers can be clocked only when system requires reading the input value, as specified in the SAMPLING field of the Control register (CTRL). The value of the pin can always be read, whether the pin is configured as input or output. If the Input Enable bit in the Pin Configuration registers (PINCFGn.INEN) is '0', the input value will not be sampled.

In PORT, the Peripheral Multiplexer Enable bit in the PINCFGn register (PINCFGn.PMUXEN) can be written to '1' to enable the connection between the peripheral functions and individual I/O pins. The Peripheral Multiplexing m (PMUXm, m = 0,...15) registers select the peripheral function for the corresponding pin. This will override the connection between the PORT and that I/O pin, connecting the selected peripheral signal to the particular I/O pin instead of the PORT line bundle.

On PIC32CM SG devices where the PORT peripheral is configured as mix-secure in H2PB, the security attribution of each pin in a PORT group is configured by the NONSEC register. If a bit in the NONSEC register is set to '0', the corresponding pin is configured as a secured pin and can only be handled by secure accesses. If a bit in the NONSEC register is set to '1', the corresponding pin is configured as a non-secured pin. Only secure accesses are allowed to write to the NONSEC register.