42.5.1 Principle of Operation

The following definitions are used throughout the documentation:

Table 42-1. Timer/Counter for Control Applications - Definitions
NameDescription
TOPThe counter reaches TOP when it becomes equal to the highest value in the count sequence. The TOP value can be the same as Period (PER) or the Compare Channel 0 (CC0) register value depending on the Waveform Generator mode in Waveform Output Generation Operations.
ZEROThe counter reaches ZERO when it contains all zeroes. (i.e. 0x00000000)
MAXThe counter reaches maximum when it contains all ones. (i.e. 0xFFFFFFFF)
UPDATEThe timer/counter signals an update when it reaches ZERO or TOP, depending on the direction settings.
TimerThe timer/counter clock control is handled by an internal source.
CounterThe clock control is handled externally (e.g., counting external events).
CC

For compare operations, the CC are referred to as "compare channels."

For capture operations, the CC are referred to as "capture channels."

There are up to 2 compare/capture (CC) channels starting from CC0 to CCn. The number of CC channels can be different on different instances of a TCC.

The Counter register (COUNT), Period registers with Buffer (PER and PERBUF), and Compare and Capture registers with buffers (CCy and CCBUFy) are 32-bit registers, on each TCC instance( if the TCC instance is a 16-bit timer/counter, the excess bits read as zero). Each Buffer register has a corresponding Buffer Valid flag in the STATUS register that indicates when the buffer contains a new value.

Under normal operation, the counter value is continuously compared to the TOP or ZERO value to determine whether the counter has reached TOP or ZERO. In either case, the TCC can generate interrupt requests, request DMA transactions, or generate events for the Event System. In Waveform Generator operation, these comparisons are used to set the waveform period or pulse width.

A prescaled generic clock (GCLK_TCCx) and events from the event system can be used to control the counter. The event system is also used as a source to the input capture.

The Recoverable Fault Unit enables event controlled waveforms by acting directly on the generated waveforms of the TCC compare channels output. These events can restart, halt the timer/counter period, shorten the output pulse active time, or disable waveform output as long as the fault condition is present. This can typically be used for current sensing regulation, and zero-crossing and demagnetization re-triggering.

The Recoverable Fault event inputs are connected to the MC0 and MC1 event lines. Only asynchronous events are used internally when fault unit extension is enabled. For further details on how to configure asynchronous events routing, refer to EVSYS – Event System.

Recoverable fault sources can be filtered and/or windowed to avoid false triggering, for example from I/O pin glitches, by using digital filtering, input blanking, and qualification options. See also Recoverable Faults.

In order to support applications for different types of motors, ballasts, LEDs, H-bridges, power converters, and other types of power switching applications, the following independent units are implemented in some of the TCC instances:
  • Recoverable faults and non-recoverable faults
See also TCC Block Diagram.

The non-recoverable fault module enables event controlled fault protection by acting directly on the generated waveforms of the timer/counter compare channel outputs. When a non-recoverable fault condition is detected, the output waveforms are forced to a preconfigured value that is safe for the application. This is typically used for instant and predictable shut down and disabling high current or voltage drives. A non-recoverable fault can be recovered only by software.

The count event sources TCCx_EV_0 connected to TCE0 input and TCCx_EV_1 connected to TCE1 input are shared with the non-recoverable fault extension. The events can be optionally filtered. If the filter options are not used, the non-recoverable faults provide an immediate asynchronous action on waveform output, even for cases where the clock is not present. For further details on how to configure asynchronous events routing, refer to section EVSYS – Event System.

References:
  • EVSYS