8.4 Analog Peripherals Considerations
This chapter provides a global view of the analog system, which is composed of the following analog peripherals:
- ADC – Analog-to-Digital Converter
- AC – Analog Comparator (and DAC)
- PTC – Peripheral Touch Controller
The analog peripherals can be connected to each other as illustrated in the block diagrams for the individual analog modules.
Important:
When an analog peripheral is enabled, each analog output of the peripheral will be prevented from using the alternative functions of the output pads. This is also true even when the peripheral is used for internal purposes.
Analog inputs do not interfere with alternate pad functions.