20.1.1 Overview

Figure 20-1. Clock Distribution Block Diagram

The PIC32CM SG00 clock system consist of the following:

  • Clock sources, that is oscillators controlled by OSCCTRL and OSC32KCTRL:
    • A clock source provides a time base that is used by other components, such as Generic Clock Generators. Example clock sources are the External Crystal Oscillator (XOSC48) and Digital Frequency Locked Loop (DFLL48M).
    • There is 1 PLL available as clock source, for system functions.
  • Generic Clock Controller (GCLK), which generates, controls, and distributes asynchronous clocks consisting of:
    • Generic Clock Generators: These are programmable prescalers that can use any of the system clock sources as a time base. The Generic Clock Generator 0 generates the clock signal GCLK_- MAIN, which is used by the Power Manager and the Main Clock (MCLK) module, which in turn generates synchronous clocks.
    • Generic Clocks: These are clock signals generated by Generic Clock Generators. They are the Peripheral Channels and serve as clocks for the peripherals of the system. Multiple instances of a peripheral will typically have a separate Generic Clock for each instance. Generic Clock 0 serves as the clock source for the DFLL48M clock input (when multiplying another clock source).
  • Main Clock Controller (MCLK)
    • The MCLK generates and controls the synchronous clocks for the system. This includes the CPU, bus clocks (AHB (Advanced High-performance Bus)), APB (Advanced Peripheral Bus) and AXI (Advanced eXtensible Interface)), as well as the Special Function Register interfaces of the peripherals. It contains clock masks that can turn on/off the user interface of a peripheral as well as prescalers for the CPU and bus clocks.

Following figure shows an example where SERCOM0 is clocked by the DFLL48M in open loop mode. The DFLL48M is enabled, the Generic Clock Generator 1 uses the DFLL48M as its clock source and feeds into Peripheral Channel 7. The Generic Clock 7, also called as GCLK_SERCOM0_CORE, is connected to SERCOM0. The SERCOM0 interface is clocked by CLK_SERCOM0_APB.

Figure 20-2. Example of SERCOM clock
To customize the clock distribution, refer to these registers and bit fields:
  • The source oscillator for a generic clock generator 'n' is selected by writing to the Source bit field in the Generator Control n, (n = 0-15), register (GCLK.GENCTRLn.SRC).
  • A Peripheral Channel m can be configured to use a specific Generic Clock Generator by writing to the Generic Clock Generator bit field in the respective Peripheral Channel m register (GCLK.PCHCTRLm.GEN).
  • The Peripheral Channel number, m, is fixed for a given peripheral. See the Mapping table in the description of GCLK.PCHCTRLm, (i.e., GCLK chapter).
  • The AHB clocks are enabled and disabled by writing to the respective bit in the AHB Mask register (MCLK.CLKMASKn).

The APB clocks are enabled and disabled by writing to the respective bit in the APB x Mask registers (MCLK.CLKMASKn).