21.5.2 External Multipurpose Crystal Oscillator (XOSC) Operation
The XOSC can operate in the following modes:
- External clock with an external clock signal connected to the XIN pin.
- Crystal oscillator with an external 4-48 MHz crystal.
The XOSC can be used as a clock source for generic clock generators. This is configured by the Generic Clock Controller.
At reset, the XOSC is disabled, and the XIN/XOUT pins can be used as General Purpose I/O (GPIO) pins or by other peripherals in the system. When XOSC is enabled, the operating mode determines the GPIO usage. When in Crystal Oscillator mode, the XIN and XOUT pins are controlled by the OSCCTRL, and GPIO functions are overridden on both pins. When in external clock mode, only the XIN pins will be overridden and controlled by the OSCCTRL, while the XOUT pin can still be used as a GPIO pin.
The XOSC is enabled by writing a '1' to the Enable bit in the External Multipurpose Crystal Oscillator Control register (XOSCCTRLA.ENABLE). To enable XOSC as an External Crystal oscillator, the XTAL Enable bit (XOSCCTRLA.XTALEN) must be written to '1'. If XOSCCTRLA.XTALEN is zero, the external clock input on XIN will be enabled.
If the External Multipurpose Crystal Oscillator Auto Gain Control Loop (XOSCCTRLA.AGC) is '1', the oscillator transconductance value (gm) will be automatically adjusted starting from lowest setting, and in most cases result in low power consumption.
The Gain control loop update rate can be controlled by the XOSCCTRLB user configuration bits.
Alternatively if the External Multipurpose Crystal Oscillator Auto Gain Control Loop (XOSCCTRLA.AGC) is '0', the user can select the oscillator operating condition by setting the transconductance value in the XOSCCTRLB register.
The XOSC will behave differently in different sleep modes, based on the settings of XOSCCTRLA.ONDEMAND, and XOSCCTRLA.ENABLE. XOSCCTRLA.ONDEMAND must be written when XOSCCTRLA.ENABLE = 0. Otherwise, the write of this bit is ignored. If XOSCCTRLA.ENABLE = 0, the XOSC will be always stopped. For XOSCCTRLA.ENABLE = 1, the table below is valid:
| CPU Mode | ON DEMAND | Sleep Behavior of XOSC and CFD |
|---|---|---|
| Active or Idle | 0 | Always run |
| Active or Idle | 1 | Run if requested by a peripheral |
| Standby | 0 | Always run |
| Standby | 1 | Run if requested by a peripheral |
| Backup | 0 | Always OFF |
| Backup | 1 | Always OFF |
After a hard reset or when waking up from a sleep mode where the XOSC was disabled, the XOSC will need a certain amount of time to stabilize on the correct frequency. This start-up time can be configured by changing the Oscillator Start-Up Time bit group (XOSCCTRLA.STARTUP) in the External Multipurpose Crystal Oscillator Control register. During the start-up time, the oscillator output is masked to ensure that no unstable clock propagates to the digital logic. The External Multipurpose Crystal Oscillator Ready bit in the Status register (STATUS.XOSCRDY) is set when the external clock or crystal oscillator is stable and ready to be used as a clock source. The INTFLAG.XOSCRDY bit is set on a zero-to-one transition of STATUS.XOSCRDY and an interrupt is generated if the External Multipurpose Crystal Oscillator Ready bit in the Interrupt Enable Set register (INTENSET.XOSCRDY) is set.
If the External Multipurpose Crystal Oscillator Auto Gain Control Loop (XOSCCTRLA.AGC) is set, and the XOSC fail to oscillate after attempting all gain settings, the External Multipurpose Crystal Oscillator Startup Fail bit in the Status register (STATUS.XOSCFAIL) is set. The INTFLAG.XOSCFAIL bit is set on a zero-to-one transition of STATUS.XOSCFAIL and an interrupt is generated if the XOSC Startup Failure bit in the Interrupt Enable Set register (INTENSET.XOSCFAIL) is set.
After the the startup time has elapsed and the External Multipurpose Crystal Oscillator did not fail oscillating, the output clock can also be monitored for failure by using the Clock Fail Detector (CFD). Refer to next section for CFD operations.