1.4 ADC Sample
This example application shows how to sample an analog input using the ADC and displays the converted samples on a serial terminal.
Description
In this application, DAC output is fed to an analog input for the ADC conversion. An
analog input is converted by a software trigger and the converted value is displayed
on the console. DAC output is changed by 0.1 V upon switch press.
Board | DAC Output Range |
---|---|
PIC32CM JH01 Curiosity Pro | 0V to 3.3V |
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/adc/adc_sample/firmware.
To build the application, refer to the following table and open the project using its IDE.
Project Name | Description |
---|---|
pic32cm_jh01_curiosity_pro.X | MPLABX project for PIC32CM JH01 Curiosity Pro Evaluation Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
Project Name | Board |
---|---|
pic32cm_jh01_curiosity_pro.X | PIC32CM JH01 Curiosity Pro Evaluation Kit |
Setting Up PIC32CM JH01 Curiosity Pro Evaluation Kit
- Analog input (AIN10) is fed from the DAC output
- Analog input “AIN10” is mapped to Port Pin “PA10” that is routed to “A4 of J803”
- DAC output “DAC” is mapped to Port Pin “PA02” that is routed to “Pin 1 of the DAC-OUT header”
- Use a jumper wire to Connect “A4 of J803” to “Pin 1 of the DAC-OUT header”
- Connect the Debug USB port on the board to the computer using a micro USB cable
Running the Application
- Open the Terminal application (Ex.: Tera term) on the computer
- Connect to the EDBG Virtual COM port and configure the serial settings as
follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
- Build and Program the application using its IDE
- Press switch to change the DAC value
- ADC input voltage changes by 0.1V when the switch is pressed, from 0.0V to 3.3V
- Refer to the table below for the switch details:
Board Switch Name PIC32CM JH01 Curiosity Pro Evaluation Kit SW0 - Console displays the ADC count and the ADC input voltage in the console as shown
below: