5.4.2 Equiv Directive
The .equiv symbol,
expression directive operates like the .equ directive, except that the assembler will signal an error
if symbol is already defined. Note that a symbol which has been referenced but not actually
defined is considered to be undefined.
Except for the contents of the error message, this directive is roughly equivalent to:
.ifdef SYM
.err
.endif
.equ SYM,VAL