13.5 Options
When you use the 32-bit archiver/librarian with command-line options, the archiver insists on at least two arguments to execute: one key letter specifying the operation (optionally accompanied by other key letters specifying modifiers) and the archive name.
xc32-ar [-]P[MOD [RELPOS][COUNT]] ARCHIVE [MEMBER...]Most operations can also accept further
MEMBER arguments, specifying archive members. Without
specifying members, the entire archive is used.
The 32-bit archiver/librarian allows you to mix the operation code P and modifier flags MOD in
any order, within the first command line argument. If you wish, you may begin the first
command line argument with a dash.
The P key letter specifies what operation to execute; it may be any of the following, but you must specify only one of them.
| Option | Function |
|---|---|
d | Delete modules from the archive. Specify the names of modules to be deleted as MEMBER...; the archive is untouched if you specify no files to delete.If you specify the |
m | Use this operation to move members in an archive. The ordering of members in an archive can make a difference in how programs are linked using the library, if a symbol is defined in more than one member. If no modifiers are used with |
p | Print the specified members of the archive, to the standard output file. If the v modifier is specified, show the member name before copying its contents to standard output. If you specify no MEMBER arguments, all the files in the archive are printed. |
q | Append the files MEMBER... into ARCHIVE. |
r | Insert the files MEMBER... into ARCHIVE (with replacement).If one of the files named in |
t | Display a table listing the contents of ARCHIVE, or those of the files listed in MEMBER..., that are present in the archive. Normally only the member name is shown; if you also want to see the modes (permissions), timestamp, owner, group and size, you can request that by also specifying the v modifier. If you do not specify a MEMBER, all files in the archive are listed.For example, if there is more than one file with the same name ( |
x | Extract members (named MEMBER) from the archive. You can use the v modifier with this operation, to request that the archiver list each name as it extracts it.If you do not specify a |
A number of modifiers (MOD) may immediately follow the P key letter to specify variations on an operation’s behavior.
| Option | Function |
|---|---|
a | Add new files after an existing member of the archive. If you use the modifier a, the name of an existing archive member must be present as the RELPOS argument, before the ARCHIVE specification. |
b | Add new files before an existing member of
the archive. If you use the modifier b, the
name of an existing archive member must be present as the RELPOS argument, before the ARCHIVE specification (same as i). |
c | Create the archive. The specified ARCHIVE is always created if it did not exist, when you requested an update. But a warning is issued unless you specify in advance that you expect to create it, by using this modifier. |
f | Truncate names in the archive. The 32-bit archiver/librarian will normally permit file names of any length. This will cause it to create archives that are not compatible with the native archiver program on some systems. If this is a concern, the f modifier may be used to truncate file names when putting them in the archive. |
i | Insert new files before an existing member of
the archive. If you use the modifier i, the
name of an existing archive member must be present as the RELPOS argument, before the ARCHIVE specification (same as b). |
l | This modifier is accepted but not used. |
N | Uses the COUNT parameter. This is used if there are multiple entries in the archive with the same name. Extract or delete instance COUNT of the given name from the archive. |
o | Preserve the original dates of members when extracting them. If you do not specify this modifier, files extracted from the archive are stamped with the time of extraction. |
P | Use the full path name when matching names in the archive. The 32-bit archiver/librarian cannot create an archive with a full path name (such archives are not POSIX compliant), but other archive creators can. This option will cause the archiver to match file names using a complete path name, which can be convenient when extracting a single file from an archive created by another tool. |
s | Write an object-file index into the archive, or update an existing one, even if no other change is made to the archive. You may use this modifier flag either with any operation, or alone. Running xc32-ar s on an archive is equivalent to running ranlib on it. |
S | Do not generate an archive symbol table. This can speed up building a large library in several steps. The resulting archive cannot be used with the linker. In order to build a symbol table, you must omit the S modifier on the last execution of the archiver, or you must run ranlib on the archive. |
u | Normally, xc32-ar
r... inserts all files listed into the archive. If you would like
to insert only those of the files you list that are newer than existing members
of the same names, use this modifier. The u
modifier is allowed only for the operation r
(replace). In particular, the combination qu
is not allowed, since checking the timestamps would lose any speed advantage
from the operation q. |
v | This modifier requests the verbose version of an operation. Many operations display additional information, such as file names processed when the modifier v is appended. |
V | This modifier shows the version number of the 32-bit archiver/librarian. |