9.5 Linker Script Command Language
Linker scripts are text files that contain a series of commands. Each command is either a keyword, possibly followed by arguments, or an assignment to a symbol. Multiple commands may be separated using semicolons. White space is generally ignored, but there are some cases where white space is significant. For instance, white space is required around operators.
Strings such as file or format names can normally be entered directly. If the file name contains a character such as a comma which would otherwise serve to separate file names, the file name may be specified in double quotes. There is no way to use a double quote character in a file name.
Comments may be included just as in C, delimited by /* and */. As in C, comments are syntactically equivalent to white space.