5.12.1
The .set noat directive prevents the assembler from using
When synthesizing some address formats, the assembler may require a scratch register. By
default, the assembler will quietly use the at ($1) register, which is reserved as an
assembler temporary by convention. In some cases, the compiler should not use that
register. The .set noat directive prevents the assembler
from quietly using that register.