4.1.1 Preprocessor Arithmetic
Preprocessor macro replacement expressions are textual and do not utilize types. Unless they are part of the controlling expression to the inclusion directives (discussed below), macros are not evaluated by the preprocessor. Once macros have been textually expanded and preprocessing is complete, the expansion forms a C expression which is evaluated by the code generator along with other C code. Tokens within the expanded C expression inherit a type, with values then subject to integral promotion and type conversion in the usual way.
If a macro is part of the controlling expression to a conditional
inclusion directive (#if or #elif), the macro must be
evaluated by the preprocessor. The result of this evaluation is often different to the
C-domain result for the same sequence. The preprocessor assigns sizes to literal values in
the controlling expression that are equal to the largest integer size accepted by the
compiler, as specified by the size of intmax_t defined in
<stdint.h>.