5.10.4 Fail Directive
The .fail expression directive generates
an error or a warning. If the value of the expression is 500 or more, xc32-as will print a warning message. If the value is less than 500, as will print an error message. The message will include the
value of expression. This can might be
useful inside complex nested macros or conditional assembly.