4.16 inline Pragma
The IAR inline pragma ensures that the following function is either in-lined or
not in-lined, based on the pragma parameter.
Suggested Replacement
There is no equivalent MPLAB XC8 pragma, but there are attributes that perform similar tasks.
Use the always_inline attribute to ensure a function is in-lined;
use the noinline attribute to prevent in-lining from taking
place.
Caveats
When indirectly calling a function using the always_inline
attribute, the compiler might or might not in-line it depending on the current
optimization level, and a failure to in-line such a call might or might not be
reported.
Examples
volatile int x;
#pragma inline=forced
void foo(void) {
x++;
}
#pragma inline=never
void __attribute__((noinline)) bar(void) {
x--;
}
int main() {
foo();
bar();
return 0;
}to
MPLAB XC8 code similar
to:volatile int x;
void __attribute__((always_inline)) foo(void) {
x++;
}
void __attribute__((noinline)) bar(void) {
x--;
}
int main() {
foo();
bar();
return 0;
}Further Information
See the Function Specifiers section in the MPLAB XC8 C Compiler User's Guide for AVR MCUs for more information on these specifiers.