4.20 object_attribute Pragma
The IAR object_attribute pragma sets object attributes to the following function
or object.
Suggested Replacement
Remove the pragma and ensure that any IAR object attributes specified with this pragma have been migrated to the MPLAB XC8 equivalent and attached to the definition of the object or function, where possible.
Caveats
None
Examples
Consider migrating IAR code such
as:
#pragma object_attribute=__no_init
char maker = 3;to MPLAB
XC8 code similar to:__persistent char maker = 3;