4.11 default_function_attributes Pragma
The IAR default_function_attributes pragma sets default segment placement, type
attributes, and object attributes for function declarations and definitions that do not
otherwise specify type or object attributes or location.
Suggested Replacement
There is no equivalent MPLAB XC8 pragma. Some of this pragma's functionality can be achieved with an attribute.
The MPLAB XC8 section attribute can be used with functions to
specify the section in which it is placed. If the Common C Interface is enabled, you
can instead use the __section specifier.
Caveats
The sections generated by this attribute are not concatenated across translation
units by the linker, and the
-Wl,--section-start,section_name=address
option, which can place a section in memory, only works with custom (non-standard)
sections.
Examples
#pragma default_function_attributes = @ "SP_SEG"
int inc(int x)
{
return x + 1;
}
#pragma default_function_attributes =to
MPLAB XC8 code similar
to:#include <xc.h>
int __section("SP_SEG") inc(int x)
{
return x + 1;
}and
build with the -mext=cci option.Further Information
See the Attributes and Ext Option section in the MPLAB XC8 C Compiler User's Guide for AVR MCUs for more information on this attribute.