4.8 constseg Pragma
The IAR constseg pragma changes the segment in which const data
is placed. Any arbitrary named segment can be provided, and default restores placement
to the default segment.
Suggested Replacement
There is no equivalent MPLAB XC8 pragma, but there is an attribute that performs a similar task.
The MPLAB XC8 section attribute can be used with a
const object to specify the section in which it is placed. If
the Common C Interface is enabled, you can instead use the
__section specifier.
Caveats
The sections generated by this attribute are not concatenated across translation
units by the linker, and the
-Wl,--section-start,section_name=address
option, which can place a section in memory, only works with custom (non-standard)
sections.
Examples
#pragma constseg=HI_MARK
const int factorySettings[] = {40, 51, 127, 0};
#pragma constseg=defaultto
MPLAB XC8 code similar
to:#include <xc.h>
const int __section("HI_MARK") factorySettings[] = {42, 15, -128, 0};and
build with the -mext=cci option.Further Information
See the Attributes and Ext Option section in the MPLAB XC8 C Compiler User's Guide for AVR MCUs for more information on this attribute.