2 Prerequisites

  1. Download the design files from: www.microchip.com/en-us/application-notes/AN5069. The design files folder contains the following subfolders:
    • Programming_Job: One programming file (.job) is provided
    • Source: Contains the source files required to complete this application note
    • Tcl_Scripts: Contains the Tcl scripts for the design
    • Softconsole: Contains Softconsole project for this design
  2. Download and install Libero SoC from: Libero SoC Documentation.
  3. Download and install the SoftConsole software from: SoftConsole.
  4. From the Libero Catalog, download the latest versions of the IP cores from the warning pop-up as shown in the following figure.
    Figure 2-1. Download New Cores Option
  5. From the Project menu, click Open project.
  6. Navigate to the mpf_an5069_v2023p1_df/mpf_10GBaseR_df/Libero_Project folder, select the Libero_Project.prjx file, and click Open.