5 Libero Design Flow
(Ask a Question)This section discusses the Libero design flow, which involves the following processes:
The following figure shows these options in the Design Flow tab.
Important: To initialize the TCM in PolarFire using the system controller, a local parameter l_cfg_hard_tcm0_en, in the
miv_rv32_subsys_pkg.v file must be changed to 1’b1 prior to synthesis. See the TCM section in the MIV_RV32 Handbook.