14.3.7 BLE OTA DFU Demo
The following BLE OTA demo steps are common for any application implementing OTA functionality.
BLE sensor application is the sample project which implements OTA functioanlity as explained in
the above steps. The current image
(ble_sensor.X.production.signed.unified_gpiobased.hex or
ble_sensor.X.production.signed.unified_timerbased.hex) with OTA
capability and new upgradable .bin (ble_sensor_1.0.0.1_enc_ota.bin) is also available
in \ble\advanced_applications\ble_sensor\precompiled_hex for your
reference.
Hardware Requirement:
Tool | Qty |
| WBZ351 Curiosity Board | 1 |
Micro USB cable | 1 |
Android/iOS Mobile | 1 |
Smartphone App: Microchip Bluetooth Data (MBD) iOS/Android app available in stores
-
Demo steps:
- To perform the OTAU, the
upgradable firmware bin file created in "Upgradable image .bin
file generation" must be stored in the MBD app. Send the
upgrdable bin file to the mail. Refer to the following screenshots to store
the image received on mail into MBD app.
- iOS Mobile:




-
Android Mobile:



- Turn on mobile Bluetooth and select “OTA DFU" tab of Microchip
Bluetooth Data App on the mobile device.

- Power On the OTA capable target device ( PIC32CX-BZ3/PIC32CX-BZ36 and WBZ35x/WBZ351 ) which was programmed
in "Programming the Application using MPLABX IDE". Device will be
advertising. Click on "SCAN" button in mobile app and the device be visible
in scanned list.

- Click on intended device from the scanned list. Mobile app will now get
connected with OTA Target device. "Connected" message will appear for a
short while.

- Click the ‘Select Image’ option to choose the available firmware file.

- The OTAU firmware image file copied in the step 1 will be visible on screen.
Click on that image.

- After confirming the FW version press OK button.

- Firmware update will be initiated and the progress will be shown in mobile
app. The process would take few seconds.

- Once the complete image is transferred, "OTA Update successfully" status
will be shown in mobile app. Click on "OK" and then device will perform
authentication of the image. If validation is successful, then system reboot
automatically.


- On bootup, device does the authentication of new image in Slot1 and then copies the new image to Slot0. Now the new image will be running from Slot0.
- To verify whether the running image on the target is newly upgraded image, follow steps 2 to 7 and check the current version.
- To perform the OTAU, the
upgradable firmware bin file created in "Upgradable image .bin
file generation" must be stored in the MBD app. Send the
upgrdable bin file to the mail. Refer to the following screenshots to store
the image received on mail into MBD app.