14.1 Bootloader

Introduction

A bootloader is a small application that can be used to upgrade firmware on a target device without the need for an external programmer or debugger. For PIC32CX-BZ3/PIC32CX-BZ36 and WBZ35x standalone bootloader, it provides below functionalities:

  • Device Firmware Upgrade over Serial(UART) interface, this is also called DFU over Serial.

  • Provide functionality support for wireless Over The Air Update, which is also called OTAU.

  • Provide various approaches to verify and authenticate firmware if enabled.

  • Display Console message if enabled

PIC32CX-BZ3/PIC32CX-BZ36 and WBZ35x Standalone Bootloader Component

PIC32CX-BZ3/PIC32CX-BZ36 and WBZ35x bootloader is a standalone Harmony component used to configure bootloader code for PIC32CX-BZ3/PIC32CX-BZ36 and WBZ35x device. See MPLAB Harmony PIC32CX-BZ System Services in Reference Documentation from Related Links to know about PIC32CX-BZ3/PIC32CX-BZ36 and WBZ35x standalone bootloader component, user can find more information as listed below:

  • Memory layout of PIC32CX-BZ3/PIC32CX-BZ36 and WBZ35x device

  • Boot memory information

  • Image metadata definition

  • Working of Bootloader

  • Flow diagram of Bootloader

  • Bootloader configuration options

  • Bootloader and DFU API usage

Functionality of Bootloader

  • Loads firmware images to embedded flash/external flash over the serial connection using a tool or python script, known as Device Firmware Upgrade (DFU)
  • Provides application protection for firmware (Secured device)
  • Upgrades application firmware to newer revision
  • Controls which application can run based on Sequence number and other metadata information embedded in the OTA image.

BootPIC32CX-BZ3/PIC32CX-BZ36 and WBZ35xloader Example Code

bootloader provided two methods to enter DFU mode, one is GPIO Trigger, another is Timber Based Trigger. Later section will have more detailed information about them.

For bootloader using GPIO Trigger method, user can find example code in wireless_apps_pic32cxbz3_wbz35\apps\bootloader\bootloader, and precompiled hex file at wireless_apps_pic32cxbz3_wbz35\apps\bootloader\bootloader\precompiled_hex\bootloader.X.production.hex

For bootloader using Timer Based Trigger method, user can find a precompiled hex file at wireless_apps_pic32cxbz3_wbz35\apps\bootloader\bootloader\precompiled_hex\bootloader_timer.X.production.hex. Since Timer Based Trigger bootloader creation is very similar to GPIO Trigger, there is no example code provided for it.

Creating Bootloader From Scratch Using MCC

This section explains the steps required by a user to configure and generate a PIC32CX-BZ3/PIC32CX-BZ36 and WBZ35x standalone bootloader from scratching using MCC. User can find the bootloader example code(GPIO Trigger) generated using MCC in the path wireless_apps_pic32cxbz3_wbz35\apps\bootloader\bootloader

Generated Bootloader example has the following configurations:
  • Enabled UART DFU

  • Enabled console to display messages

  • Enabled GPIO Trigger

  • Hardware requried is WBZ351 Curiosity Board, DFU mode is triggered by pressing SW3(GPIO PA4) on the board

  • Automatically reboot firmware after DFU is finished

WBZ351 Curiosity Board is the hardware required to run this bootloader example, the board top view is shown in figure-1.
Figure 14-1. WBZ351 Curiosity Board.

WBZ351 Curiosity Board Top View

Followings are steps to create the bootloader example(GPIO Trigger) from scratch.

Note: It is recommended for the new users of the MPLAB Code Configurator to refer MPLAB® Code Configurator (MCC) User’s Guide in Reference Documentation from Related Links.

1. Create a new harmony project. For more details, see Creating a New MCC Harmony Project from Related Links.

2. After MCC is launched, in Device Resource window, expand Harmony – Wireless – PIC32CX-BZ System Services , select Bootloader and add the component.

Figure 14-2. Device Resources Window.

Harmony-Wireless-PIC32CX-BZ System Services , select Bootloader

3. Accept all the dialog messages by clicking Yes on message prompt. This will resolve dependencies among components and add connection in the graph. Continue and click yes for next couple of options, this allows MCC to add/remove the dependencies.
Figure 14-3. Confirmation for Components Auto-activiation.

Click all YES

4. After completing auto-activation, the resulting project graph is as below.

Figure 14-4. Project Graph Window

5. Select bootloader component and satisfy the UART dependency (sercom0 for WBZ351 curiosity board).

6. Default configuration - UART DFU is connected to Port A, Pin 4; this is SW3 on WBZ351 curiosity board.

GPIO Trigger is the option to trigger DFU mode, where user needs to hold the GPIO button during reset to put the bootloader into DFU mode. Use GPIO Port and GPIO Pin option to change the port and pin based on user hardware.

Tip: Other than GPIO Trigger, another trigger option Timer Based Trigger is also provided, where bootloader will be in DFU mode for amount of time before jumping to the user application. User can change the DFU Wait Time in Milliseconds to change the amount of time. By selecting Timer Based Trigger, a 32bit timer component TC0 is asked to be activated, click YES to accept adding TC0 and accept its connection. Following figures show Timer Based Trigger options and message prompt of adding TC0.

Figure 14-5. UART connection and Bootloader configuration. satisfy the UART dependency and configure the Cootloader

7. Click on the SERCOM0 component and Configure the Baud rate if required (default is 115200).

Figure 14-6. SERCOM configuration

8. Check the configuration option for QSPI_BAUD_RATE (default is 16 MHz).

Figure 14-7. QSPI configuration

9. In project resources, select Generate option.

Figure 14-8. Generate Bootloader Code.

Press MCC Generate Button to Generate the Code

10. After project files generation has been completed, go to project properties, and select boot flash option from the header pane.

Figure 14-9. Flash Type selection

11. Configure MD_SEQ_NUM as desired.

For applications that require to always jump to the bootloader from ROM, ensure that this number is smaller than the application images

Example:

Bootloader MD_SEQ_NUM = 0x00000001

Application MD_SEQ_NUM = any value greater than 0x00000001

For applications scenario where ROM firmware needs to jump to bootloader only if there is no other valid application; make sure that the application MD_SEQ_NUM is smaller than the bootloader MD_SEQ_NUM.

Example:

Bootloader MD_SEQ_NUM = 0xFFFFFFFE

Application MD_SEQ_NUM = any value smaller than 0xFFFFFFFE

After programming MD_SEQ_NUM, select OK

Figure 14-10. Flash Type selection

12. On the IDE Tools bar, click Clean and Build Main Project to build the code.

Figure 14-11. Build Bootloader Code.

Click Clean and Build Main Project to Build Code

While generated bootloader hex file should be added to user aplication as Loadable File, they shouldn't be used alone. Followings are talking about a few simple steps need to be handled at user application side.

Configure User Application to Use Bootloader

To use Bootloader with a user application, there are a few steps to be configured at user application project. These steps are common to any user application that wants to have Bootloader capability, these steps include:

  • Add Bootloader Services component onto user application project and generate code

  • Add Bootloader as Loadable File/Project to create unified image

  • Program unified image to device.

Add Bootloader Services Component and Generate Code

Open any user application project with MPLAB X IDE, click on MCC icon on Tools bar to launch MPLAB Code Configurator to open project graph.

In Device Resource window, expand Harmony – Wireless – Driver, select Bootloader Services component and add it. This component generates the supporting linker file and MPLABX script needed for adding metadata header into application image(Project Properties is added with SignFirmware settings). Use Firmware Signature Verification API in Bootloader is the only option in Bootloader Services component. For DFU via UART, it is not necessary to enable firmware signature and verification, although user can do so if needs. While for OTAU, user must enable firmware signature and verification, by clicking on check box to Use Firmware Signature Verification API in Bootloader.

(Following project graph is just an example, user may have different graph depending on their application.)

Figure 14-12. User Application Add Bootloader Services.

Add Bootloader Services and Configure

After Bootloader Services component is added and configured, press Generate button to generate the user application code. In the generated new code, some code about bootloader service is added, as well as project’s linker script file is also automatically changed to reflect bootloader functionality.

Figure 14-13. Generate User Application Code.

Press Generate button to Generate User Application Code

Also in the updated new project, SignFirmware setting is added into Project Properties. (if not see it, try close and open MPLABX to refresh the project.) It's strongly recommended to enable Authen Method as SHA256 or ECDSA256-SHA256 in SignFirmware setting. If user choose None, since there is no firmware integrity check, if any issue happens during image saving into slot1, as new image may not be complete, the firmware may become non-functional at next restart. So None option is not secure for firmware upgrade.

ECDSA256-SHA256: firmware signature validation and data integrity check.

SHA256: firmware data integrity check.

None: no security, no integrity check.

Figure 14-14. SignFirmware - Auth Method - ECDSA256-SHA256.

Firmware signature and integrity check

Figure 14-15. SignFirmware - Auth Method - SHA256.

Firmware integrity check

Tip: Sequence Number cannot be 0x00000000 or 0xffffffff, which are invalid values.

Add Bootloader as Lodable File/Project to Create Unified Image

Once the new code is generated and configured, user need to add Bootloader as a loadable project/loadable hex file in the updated project. This enables MPLAB X IDE to merge both user application and bootloader and make an unified firmware by creating an unified image file.

To add Bootloader as loadable file, expand application project’s tree, right click Loadables, select Add Loadable File, then browse and add the bootloader hex file.

Figure 14-16. User Application Add Loadable File.

Right Click Loadables and Add Loadable File

Figure 14-17. Add Loadable File.

Select Bootloader Precompiled Hex File as Loadable File

To add bootloader as loadable project, expand application project’s tree, right click Loadables, select Add Loadable Project, then browse and add the bootloader project.
Figure 14-18. User Application Add Loadable Project.

Right Click Loadables and Add Loadable Project

Figure 14-19. Add Loadable Project.

Select Bootloader Project as Loadable Project

After Loadable File or Project is added, then on the IDE Tools bar, click Clean and Build Main Project icon to rebuild the project.
Figure 14-20. Build to Create Unified Image. Click Clean and Build Main Project to Create

Unified Image Merged Both User Application and Bootloader

After code is built, a few files is generated under path firmware\ble_sensor.X\dist\default\production. The file named as signed.unified.hex is the unified image merged with both user application and bootloader. By programing this unified image, user application will have bootloader capability. The file named as signed.bin file is the target binary image file that bootloader use for DFU. If user has any modifications on user application firmware, user can build and generate this binary file, then use bootloader to upgrade device to new image.

Program Unified Image

As mentioned above, user need to program device with unified image to make user application to have bootloader capability, to do this, on the IDE Tools bar, click Make and Program Device Main Project icon to program device, the unified image will be programmed into device.
Figure 14-21. Program Unified Image.

Click Make And Program Device Main Project to Program Unified Image

Now the device with user application will have bootloader functionality, referring the guidance in Device Firmware Upgrade Over Serial, user can run Device Firmware Upgrade by using the bootloader.